HomeServerConnector. _Connection
Properties
Methods
Abstract types
new _Connection()
Maps a connection to the HomeServer.
May not be directly instanced. An instance of the class is created by the method createConnection().
Example
Call of the 'createConnection()' method.
var conn = HomeServerConnector.createConnection("user1", "pw1", {"hostname": "192.168.123.234", "port": 443, "protocol": "wss"});
Properties
onConnect HomeServerConnector._Connection~onConnectCallback
The callback method assigned here is called as soon as a connection has been established.
Example
Connection was established
function myConnectResponse() {
...
}
...
conn.onConnect = myConnectResponse;
onDisconnect HomeServerConnector._Connection~onDisconnectCallback
The callback function assigned here is called as soon as there is no longer a connection.
Example
Connection terminated
function myDisconnectResponse(cause) {
...
}
...
conn.onDisconnect = myDisonnectResponse;
onError HomeServerConnector._Connection~onErrorCallback
The callback function assigned here is called when an error occurs.
Example
Error occurs
function myErrorResponse(error) {
...
}
...
conn.onError = myErrorResponse;
onProjectInfo HomeServerConnector._Connection~onProjectInfoCallback
The callback function assigned here is called when the information is available.
Example
conn.onProjectInfo = function(projectID) {};
onStateChanged HomeServerConnector._Connection~onStateChangedCallback
The callback function assigned here is called when the status of the current connection changes.
Example
Connection status has changed
function myStChgResponse(oldState, newState, error) {
...
}
...
conn.onStateChanged = myStChgResponse;
Methods
beginSubscription()
Initiation of a transaction to perform several subscriptions at the same time.
To optimise communication between the client and the HS, several subscriptions can be combined into one transaction. The client must then communicate with the HS only once instead of carrying out the procedure for each subscription separately.
The transaction is initiated with this method.
To end the transaction, endSubscription() is called.
Example
Subscription to 4 communication objects and one data archive in one transaction.
conn.beginSubscription():
var ko_1 = conn.getCommunicationObject("CO@1_1_1", function(err, value, isInit) {});
var ko_2 = conn.getCommunicationObject("CO@MyCoNo2", function(err, value, isInit) {});
var ko_3 = conn.getCommunicationObject("CO@TEST_CO_3", function(err, value, isInit) {});
var ko_4 = conn.getCommunicationObject("CO:31", function(err, value, isInit) {});
var arch = conn.getDataArchive("DA@MyDataArchive", function(err, data) {});
conn.endSubscription():
connect([_reconnect]) → Boolean
Establishment of connection is initiated.
An attempt to establish a connection is started immediately if a connection does not already exist.
Example
Attempts to connect to the HomeServer. Reconnection should be attempted if the connection is lost
var conn = HomeServerConnector.createConnection("user1", "pw1");
conn.connect(true);
Parameter
| Name | Type | Optional | Description |
|---|---|---|---|
|
_reconnect |
Boolean |
Yes |
true: If the connection is lost, a reconnection attempt is initiated after the Reconnect-Intervall . Defaults to |
- Returns
-
Booleantrue: An attempt to establish a connection was initiated.
false: An attempt to set up a connection could not be initiated as a connection attempt was already initiated or a connection already exists.
destroy()
All events and references will be resolved. The WebSocket will be closed.
After this method has been called this instance can no longer be used.
Example
conn.destroy();
disconnect() → Boolean
Disconnection is initiated.
Example
conn.disconnect();
- Returns
-
Booleantrue: Disconnection was initiated.
false: There is no connection.
endSubscription()
Termination of a subscription transaction.
The mode of operation is explained in the section on the method for initiating the transaction: beginSubscription().
getCameraArchive(key[, subscriptionCallback]) → HomeServerConnector._CameraArchive
Returns an instance of a camera archive.
Example
var ca = conn.getCameraArchive("CA@MyCameraArchive", function(err, data) {});
Parameters
| Name | Type | Optional | Description |
|---|---|---|---|
|
key |
String |
|
Key of camera archive |
|
subscriptionCallback |
function() |
Yes |
The Callback-Methode is called on subscription and on addition of a new entry. |
getCameraPicture(key) → HomeServerConnector._CameraPicture
Returns a camera image.
Example
var cp = conn.getCameraPicture("CP@MyCamera");
Parameter
| Name | Type | Optional | Description |
|---|---|---|---|
|
key |
String |
|
Key of camera |
getCommunicationObject(key[, subscriptionCallback]) → HomeServerConnector._CommunicationObject
Returns an instance of a communication object (CO)
Example
var co = conn.getCommunicationObject("CO@1_1_1", function(err, value, isInit) {});
Parameters
| Name | Type | Optional | Description |
|---|---|---|---|
|
key |
String |
|
Key of the communication object. |
|
subscriptionCallback |
function() |
Yes |
The Callback-Methode is called on subscription and on the change of value of the communication object. |
getDataArchive(key[, subscriptionCallback]) → HomeServerConnector._DataArchive
Returns an instance of a data archive.
Example
var da = conn.getDataArchive("DA@MyDataArchive", function(err, data) {});
Parameters
| Name | Type | Optional | Description |
|---|---|---|---|
|
key |
String |
|
Key of the data archive. |
|
subscriptionCallback |
function() |
Yes |
The Callback-Methode is called on subscription and on addition of a new entry. |
- Returns
getMessageArchive(key[, subscriptionCallback]) → HomeServerConnector._MessageArchive
Returns an instance of a message archive.
Example
var ma = conn.getMessageArchive("MA@MyMessageArchive", function(err, data) {});
Parameters
| Name | Type | Optional | Description |
|---|---|---|---|
|
key |
String |
|
Key of the message archive. |
|
subscriptionCallback |
function() |
Yes |
The Callback-Methode is called on subscription and on addition of a new entry. |
getProjectId() → (String or Undefined)
Project ID. Is only available as soon as there is a connection to the HomeServer.
Example
Query project ID
var conn = HomeServerConnector.createConnection("user1", "pw1");
...
var pid = conn.getProjectId()
- Returns
-
(String or Undefined)Project ID of the HomeServer project.
getReconnect() → Boolean
Provides the information whether a reconnection attempt should be made if the connection is lost.
This information can be set in the connect() method.
Example
Query reconnect status
var conn = HomeServerConnector.createConnection("user1", "pw1");
...
rc = conn.getReconnect()
- Returns
-
Booleantrue: If the connection is aborted, new attempts to connect should be made.
getReconnectInterval() → Number
Query reconnect attempt interval. Specification in seconds.
Example
Returns the interval in which attempts to reconnect are made if the connection was interrupted.
var conn = HomeServerConnector.createConnection("user1", "pw1");
...
ri = conn.getReconnectInterval();
- Returns
-
NumberInterval (in seconds) in which new attempts to connect are made.
getScene(key[, subscriptionCallback]) → HomeServerConnector._Scene
Returns an instance of a scene.
Example
var sc = conn.getScene("SC@MyScene", function(err, data) {});
Parameters
| Name | Type | Optional | Description |
|---|---|---|---|
|
key |
String |
|
Key of the scene |
|
subscriptionCallback |
function() |
Yes |
The Callback-Methode is called on subscription and on learning a scene. |
- Returns
getSequence(key[, subscriptionCallback]) → HomeServerConnector._Sequence
Returns an instance of a sequence.
Example
var sq = conn.getSequence("SQ@MySequence", function(err, data) {});
Parameters
| Name | Type | Optional | Description |
|---|---|---|---|
|
key |
String |
|
Key of the sequence |
|
subscriptionCallback |
function() |
Yes |
The Callback-Methode is called on subscription, on starting, stopping of the sequence or while the sequence is running. |
- Returns
getState() → Number
Status of the connection as code.
See CONNECTION_STATE.
Example
Query status
var conn = HomeServerConnector.createConnection("user1", "pw1");
...
var st = conn.getState()
- Returns
-
NumberStatus-Code.
getUniversalTimer(key[, subscriptionCallback]) → HomeServerConnector._UniversalTimer
Returns an instance of a universal timer (UT).
Example
var ca = conn.getUniversalTimer("TI@MyTimer", function(err, data) {});
Parameters
| Name | Type | Optional | Description |
|---|---|---|---|
|
key |
String |
|
Key of the timer |
|
subscriptionCallback |
function() |
Yes |
The Callback-Methode is called on subscription and on changes to the timer. |
getVacationCalendar(key[, subscriptionCallback]) → HomeServerConnector._VacationCalendar
Returns an instance of a holiday calendar.
Example
var vc = conn.getVacationCalendar("VC@MyCalendar", function(err, data) {});
Parameters
| Name | Type | Optional | Description |
|---|---|---|---|
|
key |
String |
|
Key of holiday calendar |
|
subscriptionCallback |
function() |
Yes |
The Callback-Methode is called on subscription and on changes to the holiday calendar. |
reset()
Resets all the HS objects and cancels the corresponding subscriptions.
All the HS objects generated via this connection can no longer be used after the call.
select(options[, Callback])
Returns a list of object keys with designations, as an option also the metadata of the objects.
The object options is transferred.
Example
Returns a maximum of 1000 communication objects with the tag "BM" (basement) or "Light" and no metadata
var conn = HomeServerConnector.createConnection("user1", "pw1");
...
function mySelectResponse(error, result, context) {
...
}
...
conn.select({"objectKey": "CO@*", "tags": ["BM", "Light"], "meta": False, "context": "test002"}, mySelectResponse)
Parameters
| Name | Type | Optional | Description |
|---|---|---|---|
|
options |
Object |
|
Options (see 'Properties') |
|
Callback |
function() |
Yes |
The Callback-Methode which returns the return values. |
Properties
| Name | Type | Optional | Description |
|---|---|---|---|
|
options.objectKey |
String |
|
[Filter] Object type: (see object_types). |
|
options.tags |
String |
Yes |
[Filter] List of tags. A specified tag must match the tag defined in Expert. |
|
options.search |
String |
Yes |
[Filter] List of search words. All the objects where any word begins with the specified search word in their designation or description are found. |
|
options.from |
Number |
Yes |
Position as consecutive number, beginning with '0'. Defaults to |
|
options.count |
Number |
Yes |
Maximum number of returned object keys. (Maximum value: 1000) Defaults to |
|
options.meta |
Boolean |
Yes |
true: Metadata of the selected objects are also returned. Defaults to |
|
options.context |
Object |
Yes |
The Callback-Methode returns this object unedited. |
setReconnectInterval([interval])
Set reconnect attempt interval. Specification in seconds.
Example
Sets the reconnect attempt interval to 30 seconds
var conn = HomeServerConnector.createConnection("user1", "pw1");
...
conn.setReconnectInterval(30);
Parameter
| Name | Type | Optional | Description |
|---|---|---|---|
|
interval |
Number |
Yes |
Defines the interval. Defaults to |
Abstract types
getCameraArchiveCallback(err, data)
Parameters
| Name | Type | Optional | Description |
|---|---|---|---|
|
err |
(Object or undefined) |
|
Error object |
|
data |
Object |
|
Meta information Structure (on subscription)
Structure (on addition of an entry)
Explanation
|
getCommunicationObjectCallback(err, data, isInit)
Parameters
| Name | Type | Optional | Description |
|---|---|---|---|
|
err |
(Object or undefined) |
|
Error object |
|
data |
Object |
|
Meta information Structure (on subscription and on change to value)
Explanation
|
|
isInit |
Boolean |
|
true: On subscription - false: In case of value change |
getDataArchiveCallback(err, data)
Parameters
| Name | Type | Optional | Description |
|---|---|---|---|
|
err |
(Object or undefined) |
|
Error object |
|
data |
Object |
|
Meta information Structure (on subscription)
Structure (on addition of an entry)
Explanation
|
getMessageArchiveCallback(err, data)
Parameters
| Name | Type | Optional | Description |
|---|---|---|---|
|
err |
(Object or undefined) |
|
Error object |
|
data |
Object |
|
Meta information Structure (on subscription)
Structure (on addition of an entry)
Explanation
|
getSceneCallback(err, data)
Parameters
| Name | Type | Optional | Description |
|---|---|---|---|
|
err |
(Object or undefined) |
|
Error object |
|
data |
Object |
|
Meta information Structure (on subscription)
Structure (on new teaching in)
ÿ ኘ
Explanation
|
getSequenceCallback(err, data)
Parameters
| Name | Type | Optional | Description |
|---|---|---|---|
|
err |
(Object or undefined) |
|
Error object |
|
data |
Object |
|
Meta information Structure (on subscription)
Structure (on start, stop or expiry)
Explanation
|
getUniversalTimerCallback(err, data)
Parameters
| Name | Type | Optional | Description |
|---|---|---|---|
|
err |
(Object or undefined) |
|
Error object |
|
data |
Object |
|
Meta information Structure (on subscription)
Structure (in the event of change to the timer)
Explanation
|
getVacationCalendarCallback(err, data)
Parameters
| Name | Type | Optional | Description |
|---|---|---|---|
|
err |
(Object or undefined) |
|
Error object |
|
data |
Object |
|
Meta information Structure (on subscription) and in the event of change to the holiday calendar
Explanation
|
onConnectCallback()
Example
Connection was established
function myConnectResponse() {
...
}
...
conn.onConnect = myConnectResponse;
onDisconnectCallback(cause)
Example
Connection terminated
function myDisconnectResponse(cause) {
...
}
...
conn.onDisconnect = myDisonnectResponse;
Parameter
| Name | Type | Optional | Description |
|---|---|---|---|
|
cause |
Number |
|
WebSocket status code. Reason for disconnection. |
onErrorCallback(err)
Example
Error occurs
function myErrorResponse(err) {
...
}
...
conn.onError = myErrorResponse;
Parameter
| Name | Type | Optional | Description |
|---|---|---|---|
|
err |
(Object or undefined) |
|
Error object |
onProjectInfoCallback(projectID)
Parameter
| Name | Type | Optional | Description |
|---|---|---|---|
|
projectID |
String |
|
ID of project, e.g. "20160331114440548". |
onStateChangedCallback(oldState, newState[, error])
Example
Connection status has changed
function myStChgResponse(oldState, newState, error) {
...
}
...
conn.onStateChanged = myStChgResponse;
Parameters
| Name | Type | Optional | Description |
|---|---|---|---|
|
oldState |
Number |
|
Status value before the change. |
|
newState |
Number |
|
Status value after the change. |
|
error |
Object |
Yes |
Error object. |
selectCallback(err, result, context)
Callback method of HomeServerConnector._Connection.select().
Example
Returns a maximum of 1000 communication objects with the tag "BM" (basement) or "Light" and no metadata
var conn = HomeServerConnector.createConnection("user1", "pw1");
...
function mySelectResponse(error, result, context) {
...
}
...
conn.select({"objectKey": "CO@*", "tags": ["BM", "Light"], "meta": False, "context": "test002"}, mySelectResponse)
Parameters
| Name | Type | Optional | Description |
|---|---|---|---|
|
err |
(Object or undefined) |
|
Error object. |
|
result |
Object |
|
List of object keys and designations, optionally with metadata. |
|
context |
Object |
|
The unmodified context specified on the call. |